2019-07-22 07:24 AM
Hello!
For a redesign of an already existing product we're using an STM32H743XI, which is a TFBGA240+25.
The BGA balls "B6" and "F2" are documented in two different ways in the datasheet and in CubeMX, see also attached picture.
Can you tell me which one is the correct pinout?
Datasheet: https://www.st.com/resource/en/datasheet/stm32h743xi.pdf
Kind regards,
Stefan
2019-07-22 07:41 AM
I think the Cube map is wrong, the STM32H745 data sheet is more informative.
https://www.st.com/resource/en/datasheet/stm32h745ig.pdf
2019-07-23 02:22 AM
Thank you for pointing to the 745ig datasheet. I take the datasheet information, and will ignore the CubeMX pinout, as I think it is just plain wrong.
Funny side note: It seems that there's a *third* version of the pinout of balls B6/F2 used in the Eval-Boards.
2019-07-23 05:16 AM
Some of the EVAL were designed for dual core and DSI operation, several years ago.
@STOne-32 can you check the data sheet and CubeMX databases with respect to pin naming/usage. Thanks
2019-07-31 05:27 AM
Hello,
The datasheet is the reference, the error is on CubeMX side.
It is reported internally.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.