2023-09-10 12:28 PM
Hello! I'm new to STM32 hardware, and I'm having some difficulties getting it running on my Black Pill board with an STM32F411CEU6. It has both Read and Write Protection enabled, and I am trying to disable them using STM32CubeProgrammer through an STLINK V2. However, upon trying change option bytes, it gives me a weird error.
For attempting to change read protection from value 0xFF to 0xAA it gives me this:
16:24:25:038 : Error: Expected value for Option Byte "RDP": 0xAA, found: 0xFF
16:24:25:044 : Error: Option Byte Programming failed Or modified by application after OB_LAUNCH
And similar story for trying to change the write protection values from true to false for all flash sectors:
16:26:41:386 : Error: Expected value for Option Byte "WRP0": 0x0, found: 0x1
16:26:41:391 : Error: Expected value for Option Byte "WRP1": 0x0, found: 0x1
16:26:41:395 : Error: Expected value for Option Byte "WRP2": 0x0, found: 0x1
16:26:41:399 : Error: Expected value for Option Byte "WRP3": 0x0, found: 0x1
16:26:41:408 : Error: Expected value for Option Byte "WRP4": 0x0, found: 0x1
16:26:41:416 : Error: Expected value for Option Byte "WRP5": 0x0, found: 0x1
16:26:41:428 : Error: Expected value for Option Byte "WRP6": 0x0, found: 0x1
16:26:41:436 : Error: Expected value for Option Byte "WRP7": 0x0, found: 0x1
16:26:41:441 : Error: Option Byte Programming failed Or modified by application after OB_LAUNCH
I am on Linux, and the software recognizes the MCU type and ID, so I believe the connection is good. Any help would be appreciated!
Solved! Go to Solution.
2023-10-01 8:53 AM
Hello everyone,
I ended up ordering two Nucleo L432KC boards and one new Black Pill board from Digikey. Given that Digikey's quality standards are higher than Amazon's, I figured it was a safe bet to order another one.
I've had a chance to mess around with the new Black Pill and one of the Nucleo boards and they're both working perfectly with my old programmer (or a USB cable in the case of the Nucleo board). I don't believe the old Black Pill had a counterfeit chip, but it does seem to be bricked somehow.
Thank you to @Issamos and @MikaelM for your help! I suppose the moral of the story is to order electronics off of a reputable seller rather than some random person on Amazon. I believe I will mark this as the solution, unless others have something to add.
Many thanks,
breynard
2023-09-10 1:31 PM
Hello @breynard
This problem depends on different conditions (level of read protection,Proprietary code readout protection,...) that's why I suggest you to take a look at the parts 3.6.5, 3.6.4 et 3.6.3 of the RM0383. That will give you all details you need to now. I'm suspecting that the read protection is in level 2 and that's going to be impossible to change.
Best regards.
II
2023-09-10 1:43 PM
Thank you for the prompt reply. I don't think it's in level 2 read protection, as the value reads 0xFF, not 0xCC. I remember seeing somewhere that anything but 0xAA and 0xCC is level 1 protection. Also, I don't think that will affect the ability to write to option bytes, but I could be mistaken. PCROP is enabled, and upon trying to disable it, I get the same error.
17:40:06 : Error: Expected value for Option Byte "SPRMOD": 0x0, found: 0x1
17:40:06 : Error: Option Byte Programming failed Or modified by application after OB_LAUNCH
You know far more than I do though, and if it is truly unrecoverable (either on part of the MCU or the STLINK), I can still return either or both of them.
2023-09-10 2:46 PM
2023-09-11 6:36 AM
hello @breynard ,
as suggested, you could read reference manual RM0383.
You will find page 57/844 :
"The deactivation of the SPRMOD and/or the unprotection of PCROPed user sectors can
only occur when, at the same time, the RDP level changes from 1 to 0. If this condition is not
respected, the user option byte modification is cancelled and the write error WRPERR flag
is set. The modification of the users option bytes (BOR_LEV, RST_STDBY, ..) is allowed
since none of the active nWRPi bits is reset and SPRMOD is kept active."
Best regards
Mikael
2023-09-13 6:52 PM
Hello @MikaelM
I interpret that to mean that I can only change protection option bytes at the same time I change RDP from Level 1 (which I think it is at right now with value FF) to Level 0. Upon changing this, the same error as before manifested itself:
22:47:38 : Error: Expected value for Option Byte "RDP": 0xAA, found: 0xFF
22:47:38 : Error: Expected value for Option Byte "SPRMOD": 0x0, found: 0x1
22:47:38 : Error: Expected value for Option Byte "WRP0": 0x0, found: 0x1
22:47:38 : Error: Expected value for Option Byte "WRP1": 0x0, found: 0x1
22:47:38 : Error: Expected value for Option Byte "WRP2": 0x0, found: 0x1
22:47:38 : Error: Expected value for Option Byte "WRP3": 0x0, found: 0x1
22:47:38 : Error: Expected value for Option Byte "WRP4": 0x0, found: 0x1
22:47:38 : Error: Expected value for Option Byte "WRP5": 0x0, found: 0x1
22:47:38 : Error: Expected value for Option Byte "WRP6": 0x0, found: 0x1
22:47:38 : Error: Expected value for Option Byte "WRP7": 0x0, found: 0x1
22:47:38 : Error: Option Byte Programming failed Or modified by application after OB_LAUNCH
Am I misinterpreting, or is my device bricked? Thank you so much for your time, both of you!
2023-09-14 12:30 AM
hello @breynard
could you just connect, dump option bytes and send me the log file caontaining all option bytes values ?
thanks
Mikael
2023-09-14 4:12 AM
Hello @MikaelM,
Here is the dump:
-------------------------------------------------------------------
STM32CubeProgrammer v2.14.0
-------------------------------------------------------------------
ST-LINK SN : B55B5A1A0000000053E8EE01
ST-LINK FW : V2J39S7
Board : --
Voltage : 3.27V
SWD freq : 4000 KHz
Connect mode: Normal
Reset mode : Software reset
Device ID : 0x431
Revision ID : Rev A
Device name : STM32F411xC/E
Flash size : 512 KBytes (default)
Device type : MCU
Device CPU : Cortex-M4
BL Version : 0x0
UPLOADING OPTION BYTES DATA ...
Bank : 0x00
Address : 0x40023c14
Size : 8 Bytes
[==================================================] 100%
OPTION BYTES BANK: 0
Read Out Protection:
RDP : 0xFF (Level 1, read protection of memories)
PCROP Protection:
SPRMOD : 0x1 (PCROP enabled. nWPRi bits used for PCROP protection on sector i)
BOR Level:
BOR_LEV : 0x3 (BOR OFF reset threshold level from 1.80 to 2.10 V)
User Configuration:
WDG_SW : 0x1 (Software watchdog)
nRST_STOP : 0x1 (No reset generated)
nRST_STDBY : 0x1 (No reset generated)
Write Protection:
WRP0 : 0x1 (PCROP protection active on sector i)
WRP1 : 0x1 (PCROP protection active on sector i)
WRP2 : 0x1 (PCROP protection active on sector i)
WRP3 : 0x1 (PCROP protection active on sector i)
WRP4 : 0x1 (PCROP protection active on sector i)
WRP5 : 0x1 (PCROP protection active on sector i)
WRP6 : 0x1 (PCROP protection active on sector i)
WRP7 : 0x1 (PCROP protection active on sector i)
- breynard
2023-09-15 1:23 AM
Hello, @breynard ,
thank you. I will come back to you as soon as possible on this subject.
Best regards
Mikael
2023-09-16 3:09 PM - edited 2023-09-16 3:10 PM
Hi @MikaelM,
Thank you for your continued aid in this topic! If there are any issues with the hardware, I can return and buy a new board.
Best regards,
breynard