cancel
Showing results for 
Search instead for 
Did you mean: 

ST morpho connector on NUCLEO-F030R8

Meghla
Associate II

Hi, 

In NUCLEO-F030R8 what is the pitch and overall dimensions for CN7 & CN10 ST Morpho Connector ?

Also which mating connector is used for these two connectors 

2 REPLIES 2
STTwo-32
ST Employee

Hello @Meghla and welcome to the ST Community :smiling_face_with_smiling_eyes:.

You can find all details about the CN10 and CN7 on the Bill of material of the NUCLEO-F030R8 available on NUCLEO-F030R8 - STM32 Nucleo-64 development board with STM32F030R8 MCU, supports Arduino and ST morpho connectivity - STMicroelectronics (just search for the CN7 or CN10).  Also, you will find all available dimensions on the Figure 5 of the UM1724.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Andrew Neil
Super User

It's just a standard 0.1" pitch

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.