2024-04-06 12:33 AM
hi, i got this error on stm32cubeide. I've used my board 3 weeks ago. I can't neither start the program I loaded before nor load the new program. can see Stmicroelectronics STLink Virtual COM Port COM 5 on device manager. how to solve this problem?
2024-04-06 12:57 AM
Hello @vyıbjf67 and welcome to the ST Community :smiling_face_with_smiling_eyes:.
Please check that the jumpers are correct on your board, especially the one for the ST-LINK.Then, try to connect your board with STM32CubeProgrammer. In the ST-LINK configuration area, try the following configuration:
Finally, try to connect your board.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-04-06 01:15 AM
2024-04-06 01:29 AM
ST-LINK Utility is obsolete. You have to use the STM32CubeProgrammer.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-04-06 01:31 AM
How can I use CubeIde?
2024-04-06 01:56 AM
Which board are you using? The DISCO or NUCLEO? Something else?
Make sure the pair of ST-LINK jumpers are in place.
2024-04-13 11:55 PM
Discovery and jumpers are in place.