2021-06-03 09:56 AM
Trying to have multiple ST-Link connected at one time.
Not working like I hoped.
Anyone got it working? (Multiple projects each with own STLink, all connected at same time)
Using STM32CubeIDE v1.6.1
---- My results ----
I try to set each project to a specific STLink Serial Number (I have 5 modules interconnected, and that list is growing), using:
I've written the serial number on each device by connecting one at a time and scanning for changes.
---- Suggestion ----
ST-Link serial numbers should be:
Paul
Solved! Go to Solution.
2021-06-09 09:27 AM
Works now, see notes in attached:
- MultipleSTLink=SN#.docx
I wasn't properly creating a separate Debug Configuration for each project.
2021-06-09 09:27 AM
2021-06-10 02:10 AM
Glad to see it worked out. I'll run some tests to see if I can get the same result you mentioned with the disconnected STLink!
2022-11-06 10:42 PM
You had mentioned Printed on the label (STLink/V3, STLink/Mini, etc.) in the last! Can we use a thermal Bluetooth printer to print these labels?