2024-12-15 10:46 PM - last edited on 2024-12-15 11:55 PM by SofLit
Hi,
I am having STM32U575ZI-Q development board. I have implemented a firmware with FreeRTOS with low power support where the firmware goes to the low power mode and unless there is an external interrupt, it stays in a low power mode.
Now, I want to measure the current ocnsumption when the MCU goes to the sleep mode (STOP2 mode specifically). Is there anyway I can measure the current from the STM32Cube IDE or any addtional board that can be interfaced with the development board?
Solved! Go to Solution.
2024-12-16 01:26 AM
Hi @mdalal !
Not possible for you to measure the current from the MCU through jumper JP5 with a DMM?
2024-12-16 01:26 AM
Hi @mdalal !
Not possible for you to measure the current from the MCU through jumper JP5 with a DMM?
2024-12-16 02:02 AM
Oh, do you mean that if I connect the DMM across this jumper pins, the job is done? What precision of DMM is required.
2024-12-16 02:11 AM
I am assuming that the DMM is in current measurement mode.
2024-12-16 02:26 AM - edited 2024-12-16 02:29 AM
@mdalal wrote:I am assuming that the DMM is in current measurement mode.
Yes, of course.
@mdalal wrote:Oh, do you mean that if I connect the DMM across this jumper pins, the job is done? What precision of DMM is required.
Yes. The precision of the DMM depends on your requirements. Personally I would prefer a DMM with you can at least measure 1µA.
The possible power consumption from the MCU in different situations are also described in the device datasheet. Here is a screenshot:
2024-12-16 02:41 AM
Great. I will try to get such DMM within and will let you know. You can close the ticket meanwhile.
2024-12-19 05:41 AM
Hello,
>> You can close the ticket meanwhile.
You can do that by clicking on the "Accept as Solution" button in the answer that helped you the most.