2023-10-30 4:37 PM
As the title says I just got the stm32f429I-disc1, I was really excited but I realized I couldn't start to play with it because there is no usb cable to connect a PC to the board.
Is it normal?
Solved! Go to Solution.
2023-11-01 12:01 AM
Hi @KarlY,
Let me first welcome you to the Community :)
Additional hardware accessories are needed to use the board and run your applications:
– ‘USB type A to Micro-B' cable, used to connect the board (through USB connector CN5) as USB Device to host PC.
I invite you to check the hardware environments and development recommendations required to build your application around the STM32F429-Disco through this UM1662 Getting started with the STM32F429 Discovery kit.
If you still have issues, don't hesitate to come back to the Community either with new threads or as a continuity of this one (when related to same initial topic).
Imen
2023-10-30 4:43 PM
Yes, None of the NUCLEO or DISCO boards come with cables.
You'll need a Mini-USB data cable
2023-10-30 5:56 PM
Oh okay.. does STMicroelectronics sell cable? Also which type do I need to buy ?
2023-11-01 12:01 AM
Hi @KarlY,
Let me first welcome you to the Community :)
Additional hardware accessories are needed to use the board and run your applications:
– ‘USB type A to Micro-B' cable, used to connect the board (through USB connector CN5) as USB Device to host PC.
I invite you to check the hardware environments and development recommendations required to build your application around the STM32F429-Disco through this UM1662 Getting started with the STM32F429 Discovery kit.
If you still have issues, don't hesitate to come back to the Community either with new threads or as a continuity of this one (when related to same initial topic).
Imen
2023-11-01 2:06 AM
ST isn't in that business, it's a standard Mini-B cable sort of thing you might have lying around or grab from Amazon. Bit chunkier than the Micro-B used for charging these days, but the connector is more robust and less likely to tear off at the first opportunity.