cancel
Showing results for 
Search instead for 
Did you mean: 

I am using NUCLEO-H743ZI board with STM32CubeIDE 1.7.0. When i try to debug i get(on Windows 10 machine) "No ST-LINK detected" Please connect ST-LINK and restart the debug session. " if i try the same thing (same IDE) on my Linux machine it works.Help

NThak.2
Associate

In the debug configuration if i click on ST-LINK S/N and click on Scan, i get the serial number so something seems to be working

2 REPLIES 2
NThak.2
Associate

Ok, forget it, when i connected USB port directly to PC (not via docking station) it worked

VMaft.1
Associate II

I confirm this, do not use STLink-V2 via USB HUB or docking Station. you have to use this directly into laptop/PC original USB port.