2021-09-23 06:46 AM
In the debug configuration if i click on ST-LINK S/N and click on Scan, i get the serial number so something seems to be working
2021-09-23 08:06 AM
Ok, forget it, when i connected USB port directly to PC (not via docking station) it worked
2021-11-01 06:41 AM
I confirm this, do not use STLink-V2 via USB HUB or docking Station. you have to use this directly into laptop/PC original USB port.