2025-01-19 12:09 AM
Where can i find the firmware upgrade application? I downloaded the most recent (1.28.1) stm32f4 package but under projects there's no FW_Upgrade folder.
I have an older package (1.1.0) and i can effectively find the firmware upgrade application there but i was looking for something newer, if it exists, to run the project smoothly in STM32CubeIde.
Thanks a lot and have a great day!
Omar
Solved! Go to Solution.
2025-01-19 2:41 AM
Hello @omaroski
This project is now included on the STSW-STM32068. But it is available only throw IAR, Kiel and TrueSTUDIO. So, you need to migrate it from TrueSTUDIO to STM32CubeIDE To be able to use it on the STM32CubeIDE. For that, the UM2578 should help you.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-01-19 2:41 AM
Hello @omaroski
This project is now included on the STSW-STM32068. But it is available only throw IAR, Kiel and TrueSTUDIO. So, you need to migrate it from TrueSTUDIO to STM32CubeIDE To be able to use it on the STM32CubeIDE. For that, the UM2578 should help you.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.