cancel
Showing results for 
Search instead for 
Did you mean: 

How to use X-NUCLEO-GFX02Z1 board

YordanEng
Visitor

Hi all,

 

I just bough this display extension board GFX02Z1 and have a Nucleo-F412ZG. I tried to follow the ST tutorial to write hello world on the display, but I ran into some issues. And being completely new to CubeIDE, I have no idea what's going on.

So first of all, when I choose my board in the component selector, I get this warning triangle:

YordanEng_0-1721725207272.png

I also get this triangle when I choose the application that I want to have:

YordanEng_1-1721725254735.png

I think my board uses the ST7789V, referring to the user manual, and also the memory uses SPI, so I enabled SPI1 and SPI2 in my Connectivity settings and set them to Half-Duplex mode, which resolved the issues with the LCD and Memory:

YordanEng_2-1721725475673.png

 

Can anyone help?

 

Thanks!

2 REPLIES 2
Andrew Neil
Evangelist III

@YordanEng wrote:

I just bough this display extension board GFX02Z1 !


You mean this: https://www.st.com/en/evaluation-tools/x-nucleo-gfx02z1.html ?

 

Yeah, that is the one. 

Also, I'm not sure if the application sets the pinout, but I guess it doesn't so I set it manually according to the datasheet.