2025-04-01 7:51 PM
Hi all,
I was looking at NUCLEO-U5A5 but I need support for TFT-LCD. TFT-LCD support is only available on the U599/U5A9 and better (see table below). There is also a NUCLEO-U575 but again no TFT-LCD support.
Is there a plan to make a NUCLEO-U5xx with TFT-LCD support? Thanks.
2025-04-03 8:55 AM - edited 2025-04-03 8:57 AM
Hello,
As far as I know, there is no planned Nucleo 144 board based on STM32U5x7/9.
Please have a look to these discovery boards:
STM32U5G9J-DK1 (TFBGA - DSI screen I/F - mcu @1.8V)
STM32U5G9-LQFP144-DK2 (LQFP-144 - 24bits I/F screen)
2025-04-04 7:29 PM
Correct me if I'm wrong but the STM32U5A5 and STM32U5A9 have the same pinout (LQFP144), don't they? I could buy a NUCLEO-U5A5 and replace the STM32U5A5 for an STM32U5A9 (equivalent version) and have my own NUCLEO-U5A9*.
I'll just have to make a project in STM32cubeIDE based on my custom NUCLEO-U5A9*.
This is possible, right? Assuming my soldering skills are not in the toilet :-).
(*) Not a supported STM board :)
2025-04-07 2:06 AM
Hello,
>> This is possible, right? Assuming my soldering skills are not in the toilet :-).
I think so, the pinout seems the same, and that's what I would have done myself.
But, we never tried, so I can't confirm 100%.
2025-04-09 7:13 PM
I just checked the gerbers and the NUCLEO-U575 and NUCLEO-U5A5 boards are the same. A missing xtal on the U575 vs U5A5 is no big deal but the NUCLEO-U575 is cheaper. Since I'm gonna throw away the MCU might as well get the cheaper one. Are any of these boards available without MCU? Thanks.
2025-04-10 1:21 AM
Hello,
>> Are any of these boards available without MCU?
No, there is always an MCU on the board.
2025-04-10 1:29 AM
It's not practical to have a dedicated board for every single chip variant, with every possible combination of external features.
In general, the boards use the "largest" family member - so you can prove your design on that, just ignoring the "extras" which are not in your intended chip.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.