2023-04-21 1:17 AM
I am using STM32CubeIDE with ST-LINK V3 and Segger JTAG, and this just works.
My company has now invested in a Lauterbach LA-3204, but it is not directly supported in the 'debug-settings' of CubeIDE, as ST-Link and Segger JTAG's are.
I have found out, that the TRACE32 debugger of Lauterbach can be interfaced to by using TCF in Eclipse, and I have followed those steps to do this for my CubeIDE, and it almost works, but I just can't figure out which start-script to use in my Lauterbach LA-3204.
Best regards
OleBenny
2023-05-02 8:55 AM
Hello @olebenny
First let me thank you for posting.
However, you are referring to a non ST product therefor I am not able to provide any support for it.
Maybe try to reach the vendor to provide the exact instructions.
BR,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-03-13 5:45 AM - edited 2024-03-13 5:52 AM
I'm interested in this as well.
@Semer CHERNII don't understand your response.
Of course STM32CubeID is an ST product.
Also, Lauterbach is listed in the ST Partner Program.
I think one can expect at least some form of support because of that, instead of just a "not my problem" response.