2017-07-11 09:24 AM
hello dear forum,
I bought a win10 laptop
where I tried to connect st-link/v2 adaptor
I downloaded stsw-link009 package and tried to install
however I get the message
'you have to run 64bit version of DPInst.exe on this computer'
I couldnot find this version in internet
how to proceed ?
please advice
thank you
#st-link #win102017-07-12 12:20 AM
2017-07-12 12:37 PM
hello Zhitai,
I saw it too, however...
isn't it for AMD processors ?
2017-07-13 03:02 AM
Hello,
You should launch
stlink_winusb_install.bat file that will determine the .exe to be run.
Otherwise, the installation of ST-Link Utility will install the driver automatically by the installshield.
With Regards
Imen
2017-07-13 03:31 AM
hello
please advice
2017-07-13 05:56 AM
hello thank you,
I did run '
stlink_winusb_install.bat' (even with admin rigths) in cmd window
still the message
'you have to run 64bit version of DPInst.exe on this computer'
I mean dont anybody use st-link with win10 ?
how did they do the installation ?
2017-07-13 07:02 AM
Hi
karakaya.mehmet
Please confirm which version are you using?
2017-07-13 09:25 AM
I use Windows 10 with INTEL i5 processor
I have ST-LINK / V2
I try to install stsw-link009 package
2017-07-14 02:03 AM
I have the same question�?thanks guys!
2017-07-14 03:46 AM
still unanswered
please advice