2024-04-24 04:59 AM
Hello everyone,
I own a STM32 NUCLEO G071RB. The STM CubeIDE software was working fine for a couple of weeks until I got the error message:
Target no device found
Error in initializing ST-LINK device.
Reason: No device found on target.
The board still lights up and now when connected my computer open the node G071RB file (see image attached).
I have tried all solutions from reinstalling STM32 CubeIDE to installing STM 32 programmer. But nothing is working. I have attached a file below that can help understand the problem.
Thank you for your time and consideration.
Solved! Go to Solution.
2024-04-24 12:45 PM
Hello @stmproblem348 and welcome to the Community 🙂
Check that the jumpers are correctly configured on your board.
Make sure that your ST-Link firmware is upgraded.
Try to "Connect under reset" or "power down" mode.
Check this post that may help you on how to prevent and fix debugger connection issues.
2024-04-24 12:45 PM
Hello @stmproblem348 and welcome to the Community 🙂
Check that the jumpers are correctly configured on your board.
Make sure that your ST-Link firmware is upgraded.
Try to "Connect under reset" or "power down" mode.
Check this post that may help you on how to prevent and fix debugger connection issues.
2024-04-28 08:50 PM
Thanks, one of my ST link jumper's cap went missing.