cancel
Showing results for 
Search instead for 
Did you mean: 

Debugging STM32H735G-DK: "No device found on target"

HO_MR
Associate II

STM32H735G-DK debug Question

I try to use board STM32H735G-DK.

I connected JP7 to the STLK to change the power source and connected the PC and board via CN15 with USB microB.

In STM32CubeIDE 1.13.0, I make project for the board and debug ( Fig.1 ).
I haven't added anything to the created files, but debugging failed ( Fig.2 ).
The state of the board is
・the monitor is white screen
・LD1 and LD2 is not light
・LD5 is green and LD6 is red

Fig. 1

image (4).png

 

Fig.  2

image (5).png

 I thought it might be a deadlock state, so I tried to recover from the deadlock using the STM32CubeProgrammer method as described in the documentation ( https://www.st.com/resource/en/user_manual/um2679-discovery-kit-with-stm32h735ig-mcu-stmicroelectronics.pdf 6.2.4).
When I debug after running the method, I get Figure 3 in the debug console. If I debug again I get back to Figure 2.

What was wrong with my settings?
Could you please give me some advice on how to restore the state and perform debugging?

Fig. 3

image (6).png

1 ACCEPTED SOLUTION

Accepted Solutions

Hello,

Most probably the behavior is related to an already raised issue in CubeMx in this thread.

Go to the preprocessor in your IDE and remove the USE_PWR_LDO_SUPPLY definition:

SofLit_0-1738577934049.png

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
STTwo-32
ST Employee

Hello @HO_MR and welcome to the ST Community. 
I suggest you to Check this article. It should be helpful. Also, i suggest you to update to use the Last version of the STM32CubeIDE (V1.17.0). 


Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thank you for your reply @STTwo-32.

I have updated ST32CubeIDE.

I read the article you shared and did the following three things:

- Checked PA13 (SWDIO) and PA14 (SWCLK). Fig
- Executed ST32CubeProgrammer with the settings in the article
- Set the debug configuration with the settings in the article

image (7).png

image (8).png

But after debugging, I ended up in the same state as in the question.

What else should I be suspicious of?

 

image (9).png

Hello,

Most probably the behavior is related to an already raised issue in CubeMx in this thread.

Go to the preprocessor in your IDE and remove the USE_PWR_LDO_SUPPLY definition:

SofLit_0-1738577934049.png

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Thank you for your reply, @mƎALLEm.
I really appreciate your support. I also understand the community rules.

Thank you again.