2025-02-26 7:46 AM
When I have the HC-06 powered from the board (either 3.3V or 5V) & try to upload to the board I get,
Target no device found
Error in initializing ST-LINK device.
Reason: No device found on target.
Yet when I unhook the module from the board everything uploads fine.
So, I uploaded to check my debug serial connection without the HC-06 connected, all fine.
Hook up the module, no debug . Its as if connecting it up to the power on the board knocks out the USB-ST-Link.
When I plug into the 5V - debug drops, LED3 goes out & LED1 starts flashing.
When I plug into to 3.3V - debug stops but the LEDs remain on.
I've swapped out the HC-06 module but I still get the same behaviour,
All power is being supplied by the US-ST-Link
Solved! Go to Solution.
2025-02-27 5:40 AM
Turns out I'm an *** & had shorted the 5v & GND by putting the module in the breadboard at the wrong orientation.
2025-02-26 1:28 PM
So... have the HC06 powered from something else? The USB supply via the Nucleo connector is limited.
2025-02-27 3:06 AM
What "HC-06 module", exactly?
Show your schematic of how you have this BT module connected.
Have you checked the supply voltage when it is connected?
The ST-Link should report the voltage it is seeing...
2025-02-27 5:40 AM
Turns out I'm an *** & had shorted the 5v & GND by putting the module in the breadboard at the wrong orientation.