STM32WB55CEU6 with External Battery
- July 10, 2024
- 1 reply
- 1565 views
Hello ST Community,
I am working on a circuit using the STM32WB55CEU6 micro controller and bluetooth to transmit information from one of the ADC Pins. I followed some references that have the circuit powered by a USB C connection, however in my situation it will be powered by an external battery (imagining that it is 3.3V - I could add a voltage regulator later on).
As I am not at all familiar with microcontrollers and this whole process in general, I was wondering if I could have someone check my circuit shown below. I have boxed out in the top left corner where the pads will be to solder in wires connecting to an external battery. I connected the battery's positive terminal (labeled the wire VBAT) to the VBAT pin, additionally, I've connected an outgoing +3.3V to the decoupling capacitors and the pocket programmer sections. So the ERC (electrical rules check) in KiCad V7 is giving me the warning “Both VBAT and +3.3V are attached to the same items”. I am wondering if this is the correct way to connect a battery. Any assistance on this would be greatly appreciated.
Thanks,
Rising Electrical Engineer