cancel
Showing results for 
Search instead for 
Did you mean: 

Can the ST-Link on a STM32F0Discovery be disabled?

PaulSwanson
Associate III

On the STM32F0Discovery, there's both an ST-Link chip and the main STM32F051R8T6 MCU.

Is it possible to power up and use the STM32F051R8T6 without also bringing up the ST-Link?

If so, how?

Thanks in advance.

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Guru

Power the VDD side of the JP2 jumper. Remove the JP2 jumper. Remove the CN1 CN2 jumpers.

Based on the schematic, seems like that should work.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

6 REPLIES 6
TDK
Guru

Power the VDD side of the JP2 jumper. Remove the JP2 jumper. Remove the CN1 CN2 jumpers.

Based on the schematic, seems like that should work.

If you feel a post has answered your question, please click "Accept as Solution".
PaulSwanson
Associate III

Thanks. One question. CN1 is the USB socket. Are you saying that must be desoldered?

Thanks. One question. CN1 is the USB socket. Are you saying that must be desoldered?

Sorry, I meant CN2. The jumpers that connect SWDIO/SWCLK to the ST-Link.

If you feel a post has answered your question, please click "Accept as Solution".

Thought so, thanks again. I'll give that a go. :grinning_face:

Well, as far as I can tell, this doesn't seem to work. With JP2 and both CN2 jumpers off, and voltage connected via VDD, I'm seeing some current draw but the STM32F051R8T6 doesn't seem to be working. Any other thoughts?