ST25 NFC/RFID tags and readers

Ask questions and find answers on ST25 NFC/RFID tags and readers, including connectivity implementations and antenna design.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! 3993RFID GB29768 Operating the tags

Hello!Dear ST technician!Using the chip STM32L476 +3993 provided by your company and the original code provided by the official,I have encountered a problem of operating tags. I sincerely consult you here:When the tags of GB29768 is inventory,In tag...

0693W000000W2zyQAC.png 0693W000000W303QAC.png
伟民 by Associate II
  • 2476 Views
  • 9 replies
  • 0 kudos

Resolved! ST25DV04K I2C@400kb/s compatibility?

Hello, I could not infer from the datasheet that ST25DV04K could be used at fast mode I2C speeds (400 kb/s). The datasheet states "Two-wire I2C serial interface supports 1MHz protocol". The datasheet does not mention compatibility with other I2C spee...

EJ.1 by Associate II
  • 801 Views
  • 1 replies
  • 0 kudos

Resolved! How to launch properly application to read NFC tag with an NFC03A1 nucleo attached to a NUCLEO F091RC ?

Hello,I am trying to read some NFC tag with a X-NUCLEO-NFC03A1 attached to a NUCLEO F091RC board. I am a beginner into those technology, so basically I was trying to load the sample "NFC Detect " from the package "X-CUBE-NFC3" wich can be found on ST...

KBens.1 by Associate II
  • 5001 Views
  • 31 replies
  • 0 kudos

Resolved! Is it possible to use non-blocking SPI drivers to setup RFID comms using the ST25R3911B and STM32L496 MCU

Hardware Setup: MCU: STM32L496ZG (Nucleo- L496ZG board) connected to ST25R3911B over SPI, tag is ISO15693 compliant Software: Using the rfal library and the iso15693 APIs in en.STSW-ST25RFAL001 (V2.1.2)IDE: Atollic TrueStudio V9.3.0Is it possible to ...

SDesa.1 by Associate II
  • 986 Views
  • 1 replies
  • 0 kudos

Resolved! Problems with SPI communication with ST25R95

Hi,We are facing a lot of problems with the SPI communication with an ST25R95 device. We are using as a main CPU an Silicon Labs EFR32MG13 with the next configuration: config.master    = true;      // master mode config.baudrate   = 1000000;      // ...

JCres.1 by Associate II
  • 1303 Views
  • 3 replies
  • 0 kudos

Resolved! Problem of ST25R3911 ERR_RF_COLLISION

I used ST25R3911 and ST25DV16K for nfc.​I frequently get an error message about ERR_RF_COLLISION from rfalST25xVPollerFastReadMessage.​What is the problem?​As far as I know that RF_COLLISION is happened when the NFC reader has multiple NFC Tags nerab...

HPARK.1 by Associate II
  • 2922 Views
  • 8 replies
  • 0 kudos

Resolved! What does a Security Status = 63 mean when reading a single block from a RFID tag using the ST25R3911B and ISO-15693?

Hi,Hardware Setup: MCU: XMC4200 (infineon) connected to ST25R3911B over SPI, tag is ISO15693 compliantSoftware: Using the rfal library and the iso15693 APIs in en.STSW-ST25RFAL001 (V2.1.2)I am able to successfully read the inventory, write a single b...

SDesa.1 by Associate II
  • 1355 Views
  • 1 replies
  • 0 kudos