2024-01-31 08:45 AM - last edited on 2024-02-01 01:24 AM by willzhou
I'm looking for a reference schematic where I can use the STWLC38 for Qi charging, but the Qi charging will be disabled when a USB-C is plugged in. I also need the USB-C Vbus to be isolated from the connector while the Qi charging is active.
I'd really like to have the configuration be controlled automatically by the STWLC38, if possible... Much like this from a competitive device. Is that possible?
Solved! Go to Solution.
2024-01-31 05:42 PM
Hi @BPolinske
Here is example of Wire and wireless switch circuit, it use some NMOS and PMOS.
When VBUS high, Vsys connect VBUS
When VBUS low, Vsys connect V_WLC RX VOUT
2024-01-31 05:42 PM
Hi @BPolinske
Here is example of Wire and wireless switch circuit, it use some NMOS and PMOS.
When VBUS high, Vsys connect VBUS
When VBUS low, Vsys connect V_WLC RX VOUT
2024-01-31 05:57 PM
Also i want to highligh this switch circuit advantage.
RX do not need power by external and RX do not consume any power from battery.
2024-02-01 07:57 AM - edited 2024-02-01 07:58 AM
I assume with a PMOS we can also tie V_USB_5V to the gate and the enable pin to the drain to disable the STWLC38 when USB is applied..??
2024-02-01 05:34 PM
I do not understand what circuit do you plan to use, can you draw simple picture to descript?
2024-02-02 04:38 AM
I'll generalize with a question instead. What circuit would be recommended with the STWLC38 to force the transmitter to shut off if the USB has been inserted to charge instead of using Qi?