2020-02-26 09:01 AM
We are considering using a combination of the stm32mp157 and several powerSTEP01 devices in a system with multiple stepper-motors.
The X-NUCLEO-IHM03A1 plugs into the -DK2 just fine, but the SPN3 examples only work on the F0xx, F3xx, F4xx, and L0xx series.
Attempts to port one of the examples to the stm32mp157C-DK2 have not worked.
We are approaching the GO/NOGO point of using the stm32mp1 and the powerSTEP01. Time is critical on this.
2020-03-02 11:24 AM
Well... I found that "quick and dirty"-Try, i did a couple of months ago. Main purpose was to learn about FreeRTOS and to get my Hardware working with CubeIDE, MX and TouchGFX... (Let´s say it was just a proof of concept xD) There´s also some code for a plc01a1 board inside, which isn´t usable for anybody, because i use a special adapter to "bend" some Arduino pins just for that board to solve pin conflicts with ihm03a1 😉 I´m sorry, but also forget about a lot of old comments in code and the "style". I´m not an engineer and as i said: it was just "quick and dirty" 😉
maybe it´ll help a bit …
2020-03-03 01:44 AM
Hi @karlchansen
Please pay attention that using MP1 in Production mode the resource management is perform on Linux side.
Refer to :
https://wiki.st.com/stm32mpu/wiki/Resource_manager_for_coprocessing
In order to put this aside for a first step and ease the debug, I recommend you to mature the coproc firmware using the engineering boot mode.
Please refer to :
https://wiki.st.com/stm32mpu/wiki/STM32CubeMP1_development_guidelines
Hope it help,
Olivier
2020-03-13 09:00 PM
Thanks for the file. I have been firefighting another project and am just now getting back to this one. I'll be taking a look at it this weekend.
I have also been dabbling in arduino on the M4-side of the stm32mp1. It looks like @Bumsik Kim has put a lot of work into getting the arduino core working on the stm32mp1, and the company megunolink (https://github.com/Megunolink) has created an arduino library for the powerSTEP01. I am hoping the combination works and will make my tests much simpler.