User Activity

Hi,since a couple of days i tried to get the STEVAL-ROBOT-1 up and running properly. But as i mentioned here:https://community.st.com/s/question/0D53W000003yGcdSAE/to-choice-a-kit-for-pmsmyesterday, i got more problems, than i would have expected fro...
Not really an issue, but it is worth mentioning...inside cubeIDE, i generate a new stm32 project, in target selector i select the nucleo f446re board and initialize it with the standard peripheral settings. When checking the clock configuration, i wo...
even in times of covid-19, i want to concentrate on my tasks and NOT on the tools. Buggy and faulty as usual, since a couple of days i try to bring projects, created with MCSDK 5.4.3 to work together with CubeIDE. IDE and also the integrated MX, as w...
Hi...Here the problem so far: I have a well running debug configuration, everything runs fine on target. It´s programmed into memory (using internal and external flash via qspi) and now it comes to play around with the connected (custom-) hardware. T...
Hi,I´m playing around a little bit and tried to set up a transition, as i did in TGFX 4.12... Just a very simple GUI with 1 Button on each of the 2 pages. Button on page 1 changes to page 2 and vice versa, nothing complicated. Transition is set up as...
Kudos from
Kudos given to