cancel
Showing results for 
Search instead for 
Did you mean: 

Measurement of current consumption

Nour
Associate III

Hello everyone,

I want to measure the current consumption on a STM32WB5MMDK discovery board. I've found that I had to put an ammetre on the jumper JP1, and I programmed the RGB LED to be working. However, when I put the ammetre and I power my board, I found that the current is null, and I can't find why, even if I checked the schematics and the datasheets. I was supposed to have something around 100 mA normally.

Does anyone know the reason of my problem ?

 

Thank you

Nour

1 ACCEPTED SOLUTION

Accepted Solutions

Hi,

your DMM is on AC ... 🙂

press function, to set DC measurement .

Then you will see...

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

4 REPLIES 4
MM..1
Chief II
Nour
Associate III

Yes, that is what i have followed.

I am joining the pictures

Capture d'écran 2024-07-08 095319.pngCapture d'écran 2024-07-08 095327.png

Hi,

your DMM is on AC ... 🙂

press function, to set DC measurement .

Then you will see...

If you feel a post has answered your question, please click "Accept as Solution".
Nour
Associate III

Hi, Thank you for your help!