2020-08-24 05:48 AM
Can you please share the maximum current supported by STPM32 Energy IC digital IO pin.
Solved! Go to Solution.
2020-08-31 07:06 AM
Hi @rmshub ,
I contacted a colleague who is expert in the STPM32. Following her feedback:
"The typical current with a +/-0.4V drop is about 6mA (25°C, 3.3V supply); we guarantee at least 4mA in the worst conditions (higher temp, lower Vcc)."
So my +/- 1 mA was very conservative .
You can push the sink source current up to 2 mA without concerns.
2020-08-25 01:37 AM
Hi,
According to the datasheet the high and low output levels are tested with a load current of 1 mA.
I would consider this value as operative range.
2020-08-25 01:43 AM
HI Enrico Poli,
Can I drive I/O pin as sink with 2mA. What is the maximum current supported by Vcc pin and maximum power required by STPM32 chip. (3.3V*4.6mA = 15mW)
2020-08-25 01:43 AM
HI Enrico Poli,
Can I drive I/O pin as sink with 2mA. What is the maximum current supported by Vcc pin and maximum power required by STPM32 chip. (3.3V*4.6mA = 15mW)
2020-08-27 03:34 AM
Hi @rmshub
I don't think you should exceed the 1 mA reported into the datasheet as sink/source current of the digital pins.
I'm looking for some STPM32 expert in the community. Most of the people here are focused on motor drivers and power electronics.
Meanwhile I suggest you to open a support request ticket. This way your request will be for sure forwarded to the right technical expert.
2020-08-28 02:05 AM
Hi @Enrico Poli
Thank you for information and support. I will raise the support request ticket and post an answer here if you got the information.
2020-08-31 07:06 AM
Hi @rmshub ,
I contacted a colleague who is expert in the STPM32. Following her feedback:
"The typical current with a +/-0.4V drop is about 6mA (25°C, 3.3V supply); we guarantee at least 4mA in the worst conditions (higher temp, lower Vcc)."
So my +/- 1 mA was very conservative .
You can push the sink source current up to 2 mA without concerns.
2020-08-31 07:39 AM
Hi @Enrico Poli ,
Thanks a lot for your support and time. It is simplified the my design.
Best Regards,
Ramesh