2020-09-07 10:15 AM
2020-09-07 10:32 PM
Overload conditions are buffered as long as the L9826 is being powered.
After eliminating the cause of the fault you could do a reset using the pin NRes. With parallel control, special care is required at outputs 1 and 2, see section 5.2.1 of the datasheet.
/Peter
2020-09-08 12:14 AM
Hello peter ,
thank you for reply ,
but if i am not using the parallel and i am using "Via 8-bit SPI " do i need to do reset also or the fault can be eliminated by other way,
take in consideration that when i apply a failure on a specific output pin and i remove this fault it can be eliminated if i flicker this pin one time so is that normal ?
2020-09-08 1:08 AM
Sorry, I don't understand the last sentence. What do you mean with "flicker a pin"?
2020-09-08 1:11 AM
set it with logic 0 and set it with logic 1 and then set it with 0 again