Skip to main content
FFarb.1
Visitor II
August 11, 2020
Solved

The L6472 motor driver datasheet indicates that SPI clock rise/fall times must not exceed 25nS with 30pF load. Does this mean that each L6472 presents 30pF load to SPI clock line and why is there a rise/fall time max limit??

  • August 11, 2020
  • 1 reply
  • 659 views

..

This topic has been closed for replies.
Best answer by Cristiana SCARAMEL

Hello @FFarb.1​ welcome to the ST Community.

The load of 30 pF represent the test conditions for the logic.

The timings limits have the purpose to ensure that logic does not remain too long under "indeterminate" conditions.

Let me know if I clarified your doubts.

1 reply

Cristiana SCARAMEL
ST Employee
September 7, 2020

Hello @FFarb.1​ welcome to the ST Community.

The load of 30 pF represent the test conditions for the logic.

The timings limits have the purpose to ensure that logic does not remain too long under "indeterminate" conditions.

Let me know if I clarified your doubts.

"If you feel a post has answered your question, please click ""Accept as Solution"""