cancel
Showing results for 
Search instead for 
Did you mean: 

fdcan between stm32h750 and stm32g491re

revvathi
Associate III

I am implementing FDCAN communication between an STM32H750DBK (transmitting) and an STM32G491RE (receiving) with a CAN transceiver connected on the G4 side. I am using STM32CubeIDE for development.

On the H7 side, when I load data into the FDCAN transmit buffer, I can see the correct values in the live expressions window. However, when I start execution, the data does not clear from the buffer as expected.

On the G4 side, the live expressions window shows that the receive buffer is ready and initialized with a 7-byte array, but no actual data is being received. Additionally, I am unable to run both boards simultaneously in CubeIDE due to multiple ST-LINK interfaces being detected.
also the transceiver  doesn't need a 120 ohm terminating resistor read tht it has an inbuilt resistor already

WhatsApp Image 2025-02-24 at 7.43.59 PM.jpeg

0 REPLIES 0