Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Using STSPIN220, how to detect torque increase and stall ?

Hi,I'm using STSPIN220 to drive a stepper motor with a pushrod.I only using full step mode, in order to have max. torque.I would like to detect when pushrod gets in contact with some item (increase torque), and also if stall/blocking.what would be th...

MASTERGAN rail-to-rail power supply

Hi,I am wondering if I can use the MASTERGAN with dual power supplies. i.e. high power supply +48V and low power supply -48V. In other words, the Drain of the high side GaN is +48V and Source of the low side is -48V.Regards,Mustafa

Eshua.1 by Associate
  • 750 Views
  • 0 replies
  • 0 kudos

Request of sample

Dear STM,​I need VNQ5050AK-E 31pcs of sample.Could you check that you can supply sample ?For this, I called sales office in my area but they didn't answer.​If you can't supply sample for free, I want to purchase them.I need them urgently.(I want to r...

Hkim.8 by Associate
  • 805 Views
  • 0 replies
  • 0 kudos

Need help with erroneous period readings on the STPM34.

Hi, I have the STPM34 chip connected to a 60Hz line continuously for days and it reads the frequency correctly almost all the time. However, there are instances where it would report back ~37Hz instead of 60Hz a few times in a day or sometimes it wou...

HKu.2 by Associate
  • 643 Views
  • 0 replies
  • 0 kudos

Regarding fault conditions of VNH5019A-E

Hi, I'm trying to control a motor with VNH5019A-Ehttps://www.st.com/resource/en/datasheet/vnh5019a-e.pdf​The Motor specification​s are as followsOperating Voltage : 9 ~ 16VInrush(Stall) Current at 12V : 16A​​I have a question about the following.1) O...

0693W00000D23acQAB.jpg 0693W00000D23awQAB.jpg 0693W00000D23bGQAR.png
Journey by Associate II
  • 733 Views
  • 0 replies
  • 0 kudos

Resolved! Regarding the configuration of SPV1050.

Hi,I have SPV1050 and want to use it with a solar cell. The parameters of the solar cell are listed below.Voc = 6.91 V (Open circuit voltage)Isc = 58.60 mA (Short circuit current)Pout = 307.30 mW ( Maximum deliverable power)Vload = 5.58 V (Output vol...

Reliability data and Availability of the parts

Hi ,I am using these following parts in my design,VN5E016AFH-E, VN7000AY, VN7003ALH, VN7140AJ, VN7140AS , VN7140AS12, VN820-ECould you please provide the YTEOL , MTBF, FIT data for these parts.Also, are these parts available to order now?Thanks & Reg...

RSHAR.2 by Associate II
  • 732 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.