Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

st6 eprom programmer

Posted on April 28, 2011 at 09:23hello every body, I have a problem using st6 eprom programmer with WINEE software,I use WINEE software to program st62T03C so I connect the board to PC using serial port and set all the project configuration which ar...

Slave select (NSS) pin management of SPI

Posted on April 26, 2011 at 15:10Hi all, Is there anyone who can give me some advice about the STM8S SPI? I tried to setup STM8S105 as the SPI master mode with the hardware slave select management mode which is transmit only mode. Here my source cod...

0690X00000603OUQAY.jpg

Firmware Library

Posted on April 11, 2011 at 17:08Where can I get the Discovery firmware library? The page stm8sfwlib no longer exists. Graybeard

radiation from mobile phones -> auto reset?

Posted on April 19, 2011 at 10:42Hello, I have just finished my project, but unfortunately I have a problem at the end. ;) My Stm8s Discovery is in a plastic box together with a cell phone. When the cell phone get switched on, the microcontroller re...

master by Associate II
  • 1025 Views
  • 1 replies
  • 0 kudos

Discovery board IR reciever

Posted on April 15, 2011 at 23:50I am trying to use the discovery board to work with an IR receiver to receive an IR instruction and then output onto the LCD what the instruction is. I tried looking at and trying to play with the example USART IrDA ...

Cannot communicate with STM8L-Discovery on W7-64

Posted on March 18, 2011 at 16:24I have just purchased the STM8L-DISCOVERY, I have problems getting the device communication functioning on my primary PC. I have installed all the same apps... on a secondary PC, on this PC all is OK.On my primary PC...

cd by Associate
  • 1372 Views
  • 3 replies
  • 0 kudos

multichannel ADC

Posted on July 01, 2010 at 01:39Hello all, The analog to digital example provided, ADC, uses 1 analog channel (channel 9) only.  I am working on an application and need to convert 2 voltage channels. 1) is there a way to set up the A/D to cause an i...

C standard library

Posted on April 09, 2011 at 21:59C standard libraryhello,is that possible using a vast library of standard C with STM8S in STVD.like: #include <stdio.h>#include<string.h>#include<time.h>#include<math.h>

nad by Associate II
  • 1158 Views
  • 1 replies
  • 0 kudos

Software reset in STM8

Posted on March 15, 2011 at 04:47Hi We want to perform software reset through software for the STM8L151c6T6 micro-controller. Can you please tell us the instruction or C function which can perform it? With regards Gagan Gupta #stm8l151c6t6