MAC driver using interrupts
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2007-03-15 9:38 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-17 12:30 AM
Hi,
I have successfully got the ST WEB server demo to work and am now attempting to convert the MAC driver to be interrupt driven. I am having a problem whereby an IRQ is received, but the address provided by the VIC is 0, so I just go back to reset. The init code is: INIT CODE: // From the demo ENET_InitClocksGPIO(); ENET_Init(PHY_FULLDUPLEX_100M); // Plus configure the vic. VIC_Config( DMA_ITLine, VIC_IRQ, 1 ); VIC_ITCmd( DMA_ITLine, ENABLE ); // Tried this too. //VIC_Config( ENET_ITLine, VIC_IRQ, 1 ); //VIC_ITCmd( ENET_ITLine, ENABLE ); // Clear any pending interrupt. ENET_DMA->ISR = 0xffff; // Enable the receive interrupt. ENET_DMA->IER = 0x8000; // From the demo. ENET_Start(); INTERRUPT: void ENET_IRQHandler(void) { // Just clear the receive interrupt. ENET_DMA->ISR = 0x8000; } Any ideas what I am doing wrong? Can the library code be used to generate interrupts? What is the ENET_ITLine interrupt used for. I have tried both this and DMA_ITLine. Also the problem seems to occur even with the Ethernet cable unplugged. And even if I dont enable the interrupt in the ENET_DMA->IER but still initialise the VIC. It seems the WEB demo just sets up one DMA buffer. Thanks!- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-17 12:30 AM
Watchdog setup.
SCU_APBPeriphClockConfig(__WDG, ENABLE); WDG_DeInit(); WDG_StructInit(&wdInit); wdInit.WDG_Prescaler = 0; wdInit.WDG_Preload = 47999; WDG_Init(&wdInit); WDG_ITConfig(ENABLE); VIC_Config( WDG_ITLine, VIC_IRQ, 10 ); VIC_ITCmd( WDG_ITLine, ENABLE ); WDG_Cmd(ENABLE); I have since realised that the same happens with the UART when interrupt driven. Seems whatever error I have made in not in the MAC configuration, but is more general. The MAC and/or UART will operate interrupt driven for a few minutes then the VIC returns zero as the ISR address and I get an effective reset. The SYSSTATUS contains 0x01. Some ARM processor I have used in the past will generate 'spurious' interrupt which have to be handled with a default handler. Is this the case in the STR9? Is this what could be happening? Thanks.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-17 12:30 AM
Update.
I have managed to get the ENET interrupt working now, but only if I enable interrupts and setup the VIC after calling ENET_Start() AND I stop the WDG from generating a periodic interrupt. If I wave the WDG and ENET interrupts enabled at the same time I still get the jump to 0 from the VIC supplying 0 as the vector address. Thoughts?- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-17 12:30 AM
Hi,
Can you send the watchdog initialization software for generating the periodic interrupt?- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-17 12:30 AM
Turns out this is the problem. Its working now.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-17 12:30 AM
I can successfully run an app with interrupt driven MAC, UART and periodic WDG if I handle the 'spurious' interrupts by simply clearing interrupt and not trying to process it. With moderate load I get two such interrupts per minute approximately.
Can you see anything wrong with my WDG setup?- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-17 12:30 AM
Hello,KenBarlow.I have problem with the Ethernet of STR912,I can not Ping the EvalueBorad.coulde you send your Example to me ?I preciate your help!
Best Regards!My Email :mailto:sun_yuanling@126.com