Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STVD V4.3.0 Hangs on Edit

Posted on December 16, 2011 at 09:33Hi, My setup : Windows Vista STVD V4.3.0 Cosmic C compiler STM8S Discovery board I use the example project 'stm8s-discovery_led'. I have opened the '\Project\Discover\STVD\Cosmic\Discover.stw' workspace and it bui...

joost by Associate
  • 1437 Views
  • 3 replies
  • 0 kudos

SSP problem

Posted on December 22, 2011 at 07:08I used the SSP sample code and enable SSP0 without loopback. I still get the transmitted dummy data when I send it for receving. After I test the sample code,I found that the GPIO setting cause this effect. I used...

kawumwx by Associate
  • 879 Views
  • 0 replies
  • 0 kudos

stm8s003k3

Posted on December 14, 2011 at 11:48i want to configure uart of stm8s003k3  as i have the code of uart for stm8s105c6t6 chip but when i select the stm8s003k3 chip complication  gives and error.can anyone please tell me what can i do for same code to...

IEC60730-Class C- RAM structure

Posted on December 03, 2011 at 07:59HiThis is ehsan, student of milan university, I am doing my final project in university which is relates to implementing Class c of IEC 60730. One of the routines which should be implemented, is RAM test routine v...

STVD 4.3.0 crash

Posted on November 30, 2011 at 21:51Hello,I have a problem with STVD 4.3.0. When I try to open the workspace the program crash. Behaves the same way when I create a new project and trying to modify it in the editor. The problem appeared only in vers...

Linker problem ''symbol d_imul not defined''

Posted on November 04, 2011 at 01:51I'm building a project for an STM8S208 using the Cosmic compiler (CXSTM8_32K) within ST Visual Develop.  When I link, I receive the error ''symbol d_imul not defined''.  The project was working well previously usi...

MII Management Interface variation

Posted on December 01, 2011 at 05:56We are using the Micrel KSZ8863MLL Ethernet switch with the STR912. The KSZ8863 has some extended registers (called SMI), which are accessed the same as the MII Management interface except the Opcode is '00' and n...

mykola2 by Associate
  • 967 Views
  • 0 replies
  • 0 kudos