cancel
Showing results for 
Search instead for 
Did you mean: 

SSP problem

kawumwx
Associate
Posted on December 22, 2011 at 07:08

I used the SSP sample code and enable SSP0 without loopback. I still get the transmitted dummy data when I send it for receving. After I test the sample code,I found that the GPIO setting cause this effect. I used p2.2 & p2.3 as slave I2C. When I set p2.3 GPIO_IPInputConnected_Disable, the SSP0 will function normal but slave I2C will fail. When I set p2.3 GPIO_IPInputConnected_Enable, the slave I2C function normal but SSP0 receive dummy data I send for receiving. I need slave I2C and SSP0 both on STR9. Please tell me how to solve it. Thanks.

GPIO_InitStructure.GPIO_Pin = (GPIO_Pin_0 | GPIO_Pin_1);

GPIO_InitStructure.GPIO_Direction = GPIO_PinInput;

GPIO_InitStructure.GPIO_Type = GPIO_Type_OpenCollector;

GPIO_InitStructure.GPIO_IPInputConnected = GPIO_IPInputConnected_Enable;

GPIO_InitStructure.GPIO_Alternate=GPIO_OutputAlt2;

GPIO_Init(GPIO2, &GPIO_InitStructure);

GPIO_InitStructure.GPIO_Pin = (GPIO_Pin_2 );

GPIO_InitStructure.GPIO_Direction = GPIO_PinInput;

GPIO_InitStructure.GPIO_Type = GPIO_Type_OpenCollector;

GPIO_InitStructure.GPIO_IPInputConnected = GPIO_IPInputConnected_Enable;

GPIO_InitStructure.GPIO_Alternate=GPIO_OutputAlt2;

GPIO_Init(GPIO2, &GPIO_InitStructure);

GPIO_InitStructure.GPIO_Pin = (GPIO_Pin_3);

GPIO_InitStructure.GPIO_Direction = GPIO_PinInput;

GPIO_InitStructure.GPIO_Type = GPIO_Type_OpenCollector;

GPIO_InitStructure.GPIO_IPInputConnected = GPIO_IPInputConnected_Disable;//make flash work normal but cause slave I2C abnormal

GPIO_InitStructure.GPIO_Alternate=GPIO_OutputAlt2;

GPIO_Init(GPIO2, &GPIO_InitStructure);

 /* Gonfigure SSP0_CLK, SSP0_MOSI */

 GPIO_InitStructure.GPIO_Direction = GPIO_PinOutput;

 GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4 | GPIO_Pin_5;

 GPIO_InitStructure.GPIO_Type = GPIO_Type_PushPull;

 GPIO_InitStructure.GPIO_Alternate = GPIO_OutputAlt2;

 GPIO_Init(GPIO2, &GPIO_InitStructure);

 /* Gonfigure SSP0_NSS pins */

 GPIO_InitStructure.GPIO_Direction = GPIO_PinOutput;

 GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7;

 GPIO_InitStructure.GPIO_Type = GPIO_Type_OpenCollector;

 GPIO_InitStructure.GPIO_Alternate = GPIO_OutputAlt1;

 GPIO_Init(GPIO2, &GPIO_InitStructure);

 /* Gonfigure SSP0_MISO pin GPIO2.6 */

 GPIO_InitStructure.GPIO_Direction = GPIO_PinInput;

 GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6;

 GPIO_InitStructure.GPIO_Type = GPIO_Type_PushPull;

 GPIO_InitStructure.GPIO_IPInputConnected = GPIO_IPInputConnected_Enable;

 GPIO_InitStructure.GPIO_Alternate = GPIO_InputAlt1 ;

 GPIO_Init(GPIO2, &GPIO_InitStructure);

  /* SSP0 configuration */

  SSP_DeInit(SSP0);

  SSP_InitStructure.SSP_FrameFormat = SSP_FrameFormat_Motorola;

  SSP_InitStructure.SSP_Mode = SSP_Mode_Master;

  SSP_InitStructure.SSP_CPOL = SSP_CPOL_High;

  SSP_InitStructure.SSP_CPHA = SSP_CPHA_2Edge;

  SSP_InitStructure.SSP_DataSize = SSP_DataSize_8b;

  SSP_InitStructure.SSP_ClockRate = 0;

  SSP_InitStructure.SSP_ClockPrescaler = 2;

  SSP_Init(SSP0, &SSP_InitStructure);

  /* SSP0 enable */

  SSP_LoopBackConfig(SSP0, DISABLE); 

  SSP_Cmd(SSP0, ENABLE);

#ssp
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0