Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM8S Firmware Library

Posted on January 23, 2014 at 21:38Hello, this is my first post here and my first attempt in programming an ST MCU. I today bought STM8S discovery board and it should arrive shortly.I was looking for some pointers as to where to get the firmware lib...

singhd3 by Associate II
  • 1197 Views
  • 1 replies
  • 0 kudos

ST7540 - ARDUINO - REG_DATA SPI

Posted on January 22, 2014 at 12:22Good Morning, someone could help with the SPI reg_data programming ?So right now i'm working with standard configuration but I would like modify reg_data parameter ... I would like do this using arduino ... I've a ...

andrea23 by Associate
  • 856 Views
  • 0 replies
  • 0 kudos

ADC damaged?

Posted on January 20, 2014 at 13:00STM8L152K6T6My application has one ADC input for external device connection with output volatge range in 0..2V. It works fine for a while, but once,  when external device was unplugged and plugged again, ADC channe...

igor by Associate II
  • 1027 Views
  • 0 replies
  • 0 kudos

STM8L I/O port register configuration

Posted on August 06, 2013 at 11:54I finally found the I/O port hardware register map in the hardware manual but there is no description of how to confingure the registers!Any one know where ST have hidden this vital information?The old ST7 manual ga...

STM8L Discovery USART

Posted on July 03, 2012 at 19:59i want to transmit using the stm8l152 on the stm8l discovery board. For that i have used sys config registers to remap the clk and the tx pin to the Port A. I use stvd and raisonance compiler. i cannot understand why ...

Compilation Issue

Posted on January 09, 2014 at 13:32There's an error which occurs quite commonly:  proj_name.lkfsymbol_f_NonHandled_Interrupt multiply defined in stm8l15x_it.o  While searching for the above string, there ain't any multiple definition for the same, a...

ST-LINK/V2 not seeng MCU

Posted on July 12, 2012 at 20:08Device: ST-LINK/V2 with firmware V2.J15.S4MCU: STM8L101K3T6i'm trying to connect MCU through the SWIM  in ST visual programmer but always getting ''Check the SWIM cable connection and check all the needed pin connecti...

khorght by Associate II
  • 2326 Views
  • 4 replies
  • 0 kudos

Disable pull down on MISO

Posted on January 10, 2014 at 11:01Hello,I want to disable the pull down of the internal SPI module, as I use the external slave pull down, is there a way to do it?EDIT:The MISO is driven only when NSS is released, handling NSS through software disa...

Debug (printf)

Posted on May 29, 2013 at 13:40Hi all, Just a little question about ST VD and STM8. Is it possible to use the ''printf'' or ''putchar'' functions in debug mode to display a message in a console or something like that ? (I mean without using USART) I...

ST-Link/V2 Programming Issue

Posted on September 06, 2013 at 12:39I am trying to load program using STVD (ST-Link/V2) but getting the error ''can't communicate with the device''. I am only applying Vcc and Gnd to controller + 4 wires of SWIM cable. What should I do? Do I need t...

harsh by Associate II
  • 1446 Views
  • 2 replies
  • 0 kudos