Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

use STM8S's I2C to read DS1302 questions

Posted on July 11, 2014 at 03:13I use STM8S105C6 to read DS1302;I have try the ways in the datasheet to read the DS1302's data, but it  was fail;STM8S105C6  need  ACK signal ,but DS1302 can't output ACK signal ;How can I do it;Thanks for your reply ...

timerc by Associate
  • 1052 Views
  • 1 replies
  • 0 kudos

run menu disabled in ST Visual Develop

Posted on August 01, 2014 at 12:09I'm using STVD+cosmic compiler and STM8s-discovery board, i test a little bit and go away for a long time.After i change the new computer and install STVD, cosmic,plug the USB cable to board , the board running fine...

ekpol by Associate II
  • 963 Views
  • 1 replies
  • 0 kudos

getting started with STM8S003F3

Posted on July 04, 2014 at 14:17I have to get started for STM8S003F3. I have made a custom board.1. What debugger to choose?2. What IDE, freeware preferably for c language3. Any example code to get started

SWIM DeviceID Read & ROP check-method?

Posted on February 23, 2014 at 21:47Hi, I am developing a standalone programming board for stm8 devices with SWIM interface. Development is quite far but I am still facing some questions I see nowhere answered: 1: in Flash Programming Manual it says...

at1 by Associate II
  • 2557 Views
  • 8 replies
  • 0 kudos

Where is the device ID register?

Posted on July 27, 2014 at 19:47I’m developing a programmer driver that runs through the SWIM.I now have all of my SWIM macros working, and I’m ready to move on.I am currently working with an STM8S207 device. Where is the Chip ID register? I’ve comb...

C51: Memory accesses providing strange results

Posted on July 29, 2014 at 16:27Hi,I would like to share some knowledge about a point that puzzled me for 3 days.In Keil µVision (C51), if you write the following:    char *ptr = (char *)0x8000;for accessing data located in some Flash memory for exa...

dtylski by Associate
  • 809 Views
  • 0 replies
  • 0 kudos

I2C Clock Stretching issues

Posted on July 17, 2013 at 14:30Hello, I am using STM8S105 as an I2C slave. A strange thing happens when I disable I2C_StretchClockCmd(DISBALE). When the master asks for data, the first byte is always its slave address, followed by the TX buffer. Wh...

werner by Associate
  • 1305 Views
  • 1 replies
  • 0 kudos