Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Where is the device ID register for STM8AF5268 ?

Posted on December 15, 2016 at 11:01I have to identify the device via SWIM protocol. But I cannot find any information about the existence or structure of any ID register (device ID, part ID, MCU ID, core ID, etc...)#swim #id #deviceid #id-register ...

jr by Associate II
  • 1532 Views
  • 4 replies
  • 0 kudos

Core MCU for STM8L Discovery

Posted on June 17, 2017 at 02:42Hi friends, I am new on STM. My STM8L Discovery I have bought that dont have a micro chip(STM8L152C6T6) because old owner use it for diffirent project. I want to learn this kit but hard to find STM8L152C6T6 in my coun...

Resolved! ST-LINK V2 Configuration Database

Posted on June 11, 2017 at 12:05Hello allI have an eBay ST-LINK V2 with an STM8S003F3P development board. Following the tutorial I have managed to get the project compiled without errors and set up the debugger options as instructed with the SWIM ST...

STM8L151F3 touch library 1.1.0

Posted on June 07, 2017 at 16:56¿Has anybody succeeded in using STM8 touch library with STM8L151F3?, I'm having problems getting it working with HW adquisition, I have ported STM8L151C3_Ex01 to my board and the touch pins are at 0v all the time.My ...

ADC Issue

Posted on May 25, 2017 at 16:57Hello,I'm using the STM8AL Discovery board. Im trying to get the ADC working using the ST drivers. When I initialize the code Nothing shows up in the ADC registers. Below is my initialization code:/* --- ADC --- */// I...

dwarnke by Associate II
  • 3801 Views
  • 6 replies
  • 0 kudos

Activating DAC2

Posted on March 26, 2014 at 12:25Hello, I am working with STM8L151C8 with 48 pins. To my default DAC1 output on PF0 (which works fine) I want to access to the second DAC output, which I want to have on PB6. The Ref manual says that this is possible ...

d23 by Associate II
  • 1373 Views
  • 1 replies
  • 0 kudos

STM8L152 I2C base on DMA

Posted on May 30, 2017 at 19:35Hello Everyone.I have trouble on STM8L152 with I2C through DMA. When receiving 1 data byte its receive 2 bytes 1st: some wrong  (0x1F, 0x1E, 0x0E), and second byte (looks like necessary data).In case when receive long ...

ako by Associate II
  • 1808 Views
  • 1 replies
  • 0 kudos