ST10F273 programming
Posted on January 24, 2015 at 12:32I want to know how to programm st10f273 in boot strap mode ,can anyone provide the procedure and connection diagram of the circuit?
Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
Posted on January 24, 2015 at 12:32I want to know how to programm st10f273 in boot strap mode ,can anyone provide the procedure and connection diagram of the circuit?
Posted on July 31, 2016 at 15:46Hi , I have a ST10F273M that is ACCP=0; DFB8=ACFE at one address of IFlash, i put an unprotection routine , now how i can call this function in IFlash. I can not call that via Bootstrap mode, is possible ? Do possibl...
Posted on May 07, 2008 at 21:33Unaligned memory access works ?
Posted on June 29, 2017 at 10:13hi....to program ST7FL39, i used software ST VISUAL PROGRAMMER....when i used Rlink to read STM8S103K3 with SWIM connection i can read and write what i want.......when i used ICC connection to read ST7FL39 on same pl...
Posted on June 21, 2017 at 09:10helloI am driving bipolar stepper motor using l6480. everything is fine motor is running excellent but the over current detection feature is working unpredictably. i have been disabled this feature then motor is worki...
Posted on June 28, 2017 at 09:25i am designing my own circuit by using stm8s003f3 muc... to simulate my whole design on OrCAD and make its PCB layout....plz help me....
Posted on June 26, 2017 at 22:26Hello all,I am using the 10 bits ADC converter of the STM8S105C6T6 MCU.I have a question about the maximum rating of the analog input voltage channel:in the datasheet of the MCU, it said that the max positive input vo...
Posted on June 19, 2017 at 20:12I am trying to interface USART1 with the stm8l. However I am getting a problem that whatever the value I assign to the USART1_DR , it always takes the value of 0xff no matte what. my code is as follows:(I am working w...
Posted on June 20, 2017 at 21:29 Hello, My apologize for poor English I'm working on the'simple' (as I thought) task: reading thermo sensor's indication over I2C interface. The procedure is: send command, 1 byteread sensor's answer, 3 by...
Posted on June 17, 2017 at 12:50STVD 4.3.10Cosmic V4.3.7eBay el cheapo STM8S003F3P6 (The blue one with the LED on B5)Hello all. I am having a bit of a problem with I suspect basic interrupt coding. I have the LED blinking at a variable rate with a v...