Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I am using the STM8AL3188 and am unable to read or write flash beyond 32K, even though the device has 64K flash. This occurs at address 0x10000 (flash starts at address 0x8000 making it exactly halfway). I am using IAR.

Posted on April 06, 2018 at 10:07I am using the STM8AL3188 and am unable to read or write flash beyond 32K, even though the device has 64K flash. This occurs at address 0x10000 (flash starts at address 0x8000 making it exactly halfway). I am using I...

Free STM8 Debugger for Linux?

Does anyone know of a free debugger for the STM8 for Linux? Besides SDCC there does not appear to be any free development environment for the STM8 for linux? I was happily using sdcc until I hit a bug and decided to forget about sdcc.Is there any ope...

STR912FAW46 sleep mode

Hallo allI have troubles using sleep mode with this MCU.In our application there is a hardware watchdog (STM6822), which should be restarted every 1 second.I use RTC alarm feature for periodic wake-up.The problem is that the MCU sometimes freezes and...

NFC Antenna design for CR95HF

Posted on May 28, 2015 at 19:56Hello All,I'm new here in the forum and I hope this is the right section.I would like to understand if it is possible to design the NFC antenna of the CR95HF with a separate PCB.I mean, the CR95HF is on the mother boar...

Future of Flash Application?

Posted on May 11, 2018 at 11:02Does ST have clear plans of what they are going to use to replace the Flash Configuration Application for the STNRGPF01 when Flash is finally killed off completely in 2020? 

Why the EVAL-IPFC01V1 is discountinued?

Hello,I want to know what were the problems in the EVAL-IPFC01V1 because i am using it as a reference in my design, and it will be great to know what were the mistakes in the original design.Second question: Is there any extended datasheet for the ST...