Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Option Byte Programming - Critical

Hi,I am trying to program the option byte in STM8S003 controller. I am able to do the same using STVP tool. It is not a practical method on production, so want to add the option byte config in the source code. for that I added the below code snippet....

Problem with SPI in stm8l152c6

i have configured spi in polling method.I have loaded the data into the transmit buffer and waited for TXE flag to be set.Unfortunately the flag is not being set and what could be the possbile reasons for that?I have attached the code configuration b...

Amal Babu by Associate III
  • 1385 Views
  • 4 replies
  • 0 kudos

Why pfc is not working

I have used stm l4984d ic for pfc control and got all the necessary parameters within range but still no pulse is generated by pfc ic. What can be the possible errors In my design so that I can rectify them

JDar by Associate
  • 958 Views
  • 0 replies
  • 0 kudos

STM8S003: mistake in the Reference Manual?

Hello!RM on the STM8S003: https://www.st.com/content/ccc/resource/technical/document/reference_manual/9a/1b/85/07/ca/eb/4f/dd/CD00190271.pdf/files/CD00190271.pdf/jcr:content/translations/en.CD00190271.pdfI see on the page 54, FLASH_FPR/NFPR registers...

Arlleex1 by Associate III
  • 752 Views
  • 0 replies
  • 0 kudos

Separating st-link from discovery board

Hello!If I separate stm8svldiscovery from it's stlink, do i need to do anything else, other than solder a 16MHz oscillator on the second part of the board?STM8SVLDISCOVERY board: https://www.st.com/en/evaluation-tools/stm8svldiscovery.htmlI know that...

SK.1.311 by Associate
  • 984 Views
  • 1 replies
  • 0 kudos

We are using STM8L052C6T6 . We are facing some issue on current consumptions. Below are the observations.

In Active halt mode 3v it is consuming 11uA This is fine. As we increase the voltage above 3v the current gradually increasing 3v ------->11uA3.3v------>80uA3.6v------->195uAAs per datasheet in Active halt mode it should consume 0.9uAPlease suggest...

Exception handling on ST7 micro

Greetings!I'm currently working on a project where I've taken over code for a produce that uses the ST72F321BR9 micro. This is the first time I've worked with this chip. In the past, I worked strictly with ARM core processors.I'm trying to figure o...

GAldr by Associate
  • 1473 Views
  • 3 replies
  • 0 kudos