Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VN380SP

I can't find any information about VN380SP at the st.com siteIs VN380SP discontinued? Deprecated product?

AShab.10 by Associate
  • 680 Views
  • 0 replies
  • 0 kudos

STM8: mistake in datasheet?

Good morning.STM8S003: https://www.st.com/resource/en/datasheet/DM00024550.pdfOn a page 45 under table 15 (quote):"2. Do not use more than one remapping option in the same port. It is forbidden to enable both AFR1 and AFR0."Here first part of the sen...

Arlleex1 by Associate III
  • 772 Views
  • 1 replies
  • 0 kudos

Hi, I have Design a Relays Based AC Switch Board using STM8s003 and ESP01. When I connect even a small resistive load then the controller resets during relays switching.... i dont know whether where is the problem in my design?

 >>The Board is working fine when there is no AC (220v) load Connected; but with AC Load Connected, then MCU resets during switchingSame type of switch boards are available online containing stm8 but i havent experienced these boards regarding such a...

SKhan.4 by Associate
  • 816 Views
  • 0 replies
  • 0 kudos

Is 23257-B related to ST72324?

I am trying to identify this 32 pin chip (23257-B) used in an automotive application (see picture). I am unable to locate any spec sheets. I am pretty sure it is a variant of the STMicroelectronics ST72324 8-bit microcontroller.  Can anyone confirm a...

0690X000006E1KCQA0.jpg
DEdwa by Associate
  • 725 Views
  • 0 replies
  • 0 kudos