Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I need to program the ST8L101F3P6 with ST viual

hi,       I am using ST8l101F3P6 microcontroller.I have used ST Visual develop with Cosmic compiler.I Programmed and compiled successfully.but I can not Program the controller with ST visual programmer..when I try to program it asks to check the conn...

karthik.b by Associate II
  • 2611 Views
  • 4 replies
  • 0 kudos

stm8s_adc1 SPL files throwing compiler errors

Further to my previous message I have setup a new STVD workspace, included stm8s.h and just stm8s_adc1.c and .h, setup processor etc and get 150+ compiler errors on stm82_adc1.c just as if the header file was not specified but it is. So having reduce...

BCowa by Associate II
  • 889 Views
  • 0 replies
  • 0 kudos

Why I fill wrong TIM2 registers when I run STM8S103 with en.stsw-stm8069 (I see in debug mode) TIM2. IDE=IAR ??

Hello everyone, I am running STM8S103F3P with IAR. I downloaded this: en.stsw-stm8069.In IAR chosed my micro STM8S103F3P. But as I see in debug mode I fill wrong register (TIM2) at init TIM2 regs. It seems setup (config) in IAR is wrong or I did som...

L9825 SPI Control Not Functioning

I am attempting to set the output states of an L9825 using its SPI interface, but no matter what byte is transmitted, the returned diagnostic byte is 0x88 and the output state is unaltered.clock frequency : 1 MHzclock polarity: lowclock phase: data c...

MBoren by Associate II
  • 952 Views
  • 0 replies
  • 0 kudos