Programming an in circuit STM8S105K6T6C MCU Via UART
Using STLINK-V3SET. Please Note in circuit STM8S105K6T6C embedded board has these pins GND, RX, TX , VCC. Many thanks
Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
Using STLINK-V3SET. Please Note in circuit STM8S105K6T6C embedded board has these pins GND, RX, TX , VCC. Many thanks
1. I am using Stm8s003f3.In it a slave SPI device is connected, which only inputs data, it dont output any data so MOSI is only used.2. My question is can I use remianing MISO pin as GPIO? since MOSI is used after configuring SPI, will it automatcial...
Hello Respective,I am using STM8l052C6 device for my product, I want to design my own bootloader for the same.Is it possible, as I didn't find any guideline for the same in relavent documents.
Hi. I'm using an STMTL52F4 20-pin MCU that I've programmed to immediately enter HALT mode on startup with the halt() command. Although the documentation says that the chip consumes only 0.4uA in this state, when I put a multimeter in series with the ...
void main(void) { uint16_t tmpcnt = 0; uint8_t tmpcntrl, tmpcntrh; setup_pins(); CLK_PeripheralClockConfig(CLK_Peripheral_TIM2, ENABLE); TIM2->PSCR = TIM2_Prescaler_1; TIM2->ARRH = 0; TIM2->ARRL = 1; TIM2->CNTRH = ...
Hi.Regarding I2C Bus busy problem. I am using alternative pins (PB4 and PB5), as I have the small chip with fewer pins.Option bits are set, and verified.However even at power up the BUSY bit is set. It is set through configuration of the I2C peripher...
#include <stm8l15x.h> #include <stm8l15x_pwr.h> void main(void) { GPIO_Init(GPIOA, GPIO_Pin_All, GPIO_Mode_Out_PP_Low_Fast); GPIO_Init(GPIOB, GPIO_Pin_All, GPIO_Mode_Out_PP_Low_Fast); GPIO_Init(GPIOC, GPIO_Pin_All, GPIO_Mode_Out_PP_Low_Fast); ...
Hi. I'm using STVD v 4.3.12 with an STMTL52F4 MCU. Debug building works just fine. However, when I switch over to a Release build (changing nothing else), it fails to compile, reporting that it can't open an include file it was able to find before. C...
We are developing a product that uses segment_LCD using stm8l052r8.There was no problem when developing with com4+seg28There was a problem when developing with com8+seg24.When you turn on the entire screen, all the text on the screen comes out well.I...