Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Impossible to re-open my old projects :

When I reimport the project from my PC or try to open it in the cloud. I have a short view to the design and next always the same question : "Sign in with your corportate ID" and then I can do nothing

PPito.1 by Associate II
  • 7796 Views
  • 11 replies
  • 0 kudos

What does the STM8 TIM3_BKRConfig() function do?

As a newbie I'm struggling to understand the following line of code:TIM3_BKRConfig(TIM3_OSSIState_Enable,TIM3_LockLevel_1,TIM3_BreakState_Enable,TIM3_BreakPolarity_High,TIM3_AutomaticOutput_Enable);Introductory material that I've found on timers/PWM ...

PiSquared by Associate II
  • 1472 Views
  • 1 replies
  • 0 kudos

Minimum supply voltage of M24M02

Hello,The minimum supply voltage for the M24M02 is 1.8 V (range of 1.8 V to 5.5 V). The Power Integrity Simulations ​of our hardware design showed a voltage of 1.7921 V @ pin A2 (VCC). This is a drop of almost 8 mV.I know, 8 mV below 1.8 V is almost ...

RAtem.1 by Associate
  • 1258 Views
  • 2 replies
  • 0 kudos

STM8S005K6 Bootloader no responding at data

HiI have a problem when I start writing the first page of the program.I am running at 115200 8 data bit, 1 stop, no parity.I am running in ECHO mode, meaning I return all bytes from the bootloader.I have send the SYNC byte, at power up, and getting a...

HMoel.1 by Associate II
  • 1557 Views
  • 2 replies
  • 0 kudos

Which antenna connection is right?

Hello,​I am currently working on custom BLE sensor for my university project and whole design is based on your ​STEVAL-BCN002V1B evaluation board. When it came to antenna routing I discovered that your schematic diagram and antenna's (ANT016008LCS244...