Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! There is a problem with software installation

After downloading the stToolset_pack42 installation package from the official website, it will get stuck when installing to the following steps, resulting in the failure of installation. May I ask how to solve this problem?

0693W000004KBe8QAG.png
李YY.1 by Associate II
  • 1171 Views
  • 1 replies
  • 0 kudos

How to initialise the RTC on STM8L151K4T6

Hi All, This is my first MCU project attempt and figured I would build a 7-segment clock. I have managed to write a little bit of code to configure the GPIOs in the way that I want them as well as the system clock, but I cannot for the life of me fig...

JEdmu.1 by Associate
  • 900 Views
  • 0 replies
  • 0 kudos

Resolved! STM8 Frequency Counter

Hello, I'm trying to implement a simple frequency counter. The idea is I have some external signal sitting at 6MHz, and I want to measure it by simply starting the TIM1 counter, waiting 1ms (delay), then reading the count, which I'd expect to be abou...

SBrow.1 by Associate II
  • 1746 Views
  • 1 replies
  • 1 kudos