E-L9823013TR Looking alternate for the above part
We are corrently using E-L9823013TR driver Looking for alternate for the same. Kindly suggest us if you have alternates.
Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
We are corrently using E-L9823013TR driver Looking for alternate for the same. Kindly suggest us if you have alternates.
Data Sheet of IC ATIC39-B4 A2C08350
Hello everyone,I have a problem with touch sensing on STM8L151K4, It is impossibe to increase number of touch key to 10.I have to put each key in a bank for it to work. ie my project needs 8 touch keys and consumes 8 banks.I tried my best to put mult...
How to store more than one 32 bit variable in eeprom memory in while loop and also to receive downlink?Here,I have attached the code too.
I tried this code on STM8S001J3 with 8 pins:/* MAIN.C file * * Copyright (c) 2002-2005 STMicroelectronics */ //#include “stm8s.h�? /*main() { while (1); } */ #include "STM8S.h" void clock_setup(void); void GPIO_setup(void); void TIM1_setu...
We are getting massive ammounts of emissions from the D0 SDIO pin with 120mhz and resonant freqs. The pins for SDIO have been set to AF but nothing else has been setup register wise yet, the circuit was taken from the appnotes with the 3v3 pullups on...
STM8S103 not reading data in SPI Slave mode sent by STM8S103 SPI master. Even all the configurations of Slave and Master are the same. I am using IAR IDE.Please review the code of both Slave and Master and help me STM8S SLAVE CODE:#include "STM8S.h"...
Trying to work around chip shortage with a single executable
The circuit works fine with 5v/9V adapter supply but when we connect with 9v Battery controller could not work as expected. I have assembled stm8s103f3p6 break out board with my circuit, which have below gpio connections! //Chip_Pin_No. Pin Name...
Hi, I am developing with STM8S003F3.I want to store user-specific information somewhere in the flash and read only that area with ST-LINK.Is there such a way?Regards, Gotoda