Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! EMIF08-LCD04M16 PIN OUT?

I am looking to get confirmation on the pin out of EMIF08-LCD04M16 in QFN package. The datasheet makes no mention of this. I assume that it is a pass through type, where pins opposite each other are connected through the filters, and that the exposed...

JSten.3 by Associate
  • 1097 Views
  • 1 replies
  • 0 kudos

Interrupt Handler execute issue on NUCLEO-8S208RB

I downloaded the blink LED demo from ST and loaded in that nucleo board to check out how things worked, soon I found out that every time when I pressed the "USER" Button (Connected to PE4), It won't be able to successfully switch to next blink patter...

TSu.1 by Associate III
  • 947 Views
  • 0 replies
  • 0 kudos

STWINKT1B connect to MQTT through 5g wifi

Hi, I have a STWINKT1B board which I want to connect to my organization's 5ghz Wi-Fi to be able to send sensor logs to MQTT. To do this what additional hardware do I require (as the WIFI expansion pack for this board only supports 2.4ghz). And is th...

NRaha.1 by Associate II
  • 885 Views
  • 0 replies
  • 0 kudos