Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! What is the body marking of M24C32-RMN6TP

Please help to provide the body marking surface of this material. There is no description in the spec, so it is impossible to confirm whether the material used is correct. Thank you! MANUFACTURER: ST MANUFACTURER PN: M24C32-RMN6TP 

YW.1 by Associate II
  • 3028 Views
  • 4 replies
  • 0 kudos

STM8L151K6:COMP2...Does closing WINDWE analog switch (for Window mode) disconnect COMP1 non-inverting input from AS14 in the analog switch matrix?

Using the Cosmic IDE, I have the non-inverting input of COMP1 driven from PA4 by closing RI_AnalogSwitch_14 and RI_AnalogSwitch_0 and enabling RI_IOSwitch_3. I have COMP1 configured for COMP_Edge_Rising and the COMP1 interrupt is enabled. I see inter...

REdmo.1 by Associate III
  • 1726 Views
  • 2 replies
  • 0 kudos

Resolved! I would like to kwow if my SM6T18A/CA on the input connector of my product is compliant with the no destruction of my electronic which is located just after when fast Transient 61000-4-4 is applied.

Hi Sir,I currently use a SM6T18A/CA on the 12V+/- 5% power supply input of my product.After this protection are located many electronic components with absolute maximum rating voltage levels (continuous) given from 13,2V to 18V. After applying the tr...

NAnth.2 by Associate
  • 1774 Views
  • 2 replies
  • 0 kudos

Able to control STM8S nucleo board, but same code to chipset on my own board does nothing. How can I debug?

I use STVD with the cosmic compiler, SPL library and STVD to flash. I am able to control the STM8S208RB Nucelo board with this setup, and verify the board is functioning correctly.I then lay out a PCB with a STM8S003F in a TSSOP-20 package. The layou...

PBeve.1 by Associate
  • 1271 Views
  • 0 replies
  • 1 kudos

How do I replace the memory that came with the EVAL-SC003V1 with the STM32CubeProgrammer? It firstly erased the memory on the EVAL-SC003V1 because the default is to not skip flash erase before programming.

I'm not certain that the default memory file for the EVAL-SC003V1 was provided in any of the zip files I downloaded. Is replacing the memory sectors between the STUSB005 GUI the correct way to program the EVAL-SC003V1 board? The sectors from the GUI ...

DMich.3 by Associate
  • 1061 Views
  • 0 replies
  • 0 kudos

STM8L050J3 wfe() wakeup using TIM2 timer.

Good morning. I've been trying for a while to put the MCU in low power with the wfe() instruction and wake it up with TIME2 but the MCU gets stuck in wfe() and doesn't wake up. With the debugger active it seems to work even if it doesn't respect the ...

GBran.2 by Associate II
  • 4018 Views
  • 4 replies
  • 0 kudos