2009-08-10 01:38 AM
2009-08-10 01:38 AM
Hello,
I just started a project that uses STR7 microcontroller. The software is built with Anglia IDE and the STR7 toolchain associated with it. This is a new project for me. I used to work with Keil compilers with 8051 and I used to use Source Insight for editing code. However in this new project, the company wants to use free tools. I chose Eclipse as an IDE because I use it for Java development and I quite like it. My question is, can I edit, build and debug my CPP source code for STR7 with Eclipse using the STR7 toolchain from Anglia? Is there a support for this toolchain in Eclipse? Although I Googled a lot, I couldn't find any information about it. I'll be grateful if anyone could help.