2024-12-28 10:40 AM
Windows 11 / IDE Version: 1.17.0 / Build: 23558_20241125_2245 (UTC)
I tried changing the IDE's theme from classic to Dark, Light, and even Eclipse Marketplace themes. I always get some weird visuals. If I have one tab selected and hover over another, the selected tab duplicates and replaces the tab hovered over (refer to screenshot). Another bug makes the tabs disappear entirely when hovered over. Also, the maximize and minimize icons are crossed out with a white line. This only happens with any theme, but the classic one. Window > Preferences > Appearance > Theme. I restarted the IDE after changing the theme, but it didn't make a difference.
2024-12-30 12:23 AM
Hello @Ziimag
First, let me thank you for posting. Consider reinstalling the IDE. Make sure to back up your workspace and settings before doing so, and check if the issue persists. I will be waiting for your feedback
THX
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.