2024-12-18 3:34 AM
Having upgraded CubeIDE to version 1.17.0 using 'check for updates' and found it didn't work for my project, I tried to go back to version 1.15.1 using the revert button. After running this, the IDE would not start and give an error message indicating that the ~/.eclipse/com.st.stm32cube.ide.mcu.rcp.product_1.15.1_139064214_linux_gtk_x86_64/configuration/config.ini file had blank filenames. I found what looked like a complete file at /opt/st/stm32cubeide_1.15.1/configuration/config.ini which I copied to the above location and which then worked OK.
2024-12-18 3:37 AM
Hello @TJack.2 ,
Better to ask a question / describe the issue then add a comment where you provide the solution and accept it as solution.
Thanks